Digi-Key Weather Center


Positioned on the roof of Digi-Key's 600,000 square foot Product Distribution Center in Thief River Falls, Minnesota in July 2010, the Digi-Key Weather Center tracks the most dramatic of weather changes year-round. The Digi-Key Weather Center was developed to demonstrate connectivity to customers by using products available and supported by Digi-Key. This project is a collaborative effort by members of Digi-Key's Design Support Services team.

Please direct questions and comments to Digi-Key's Application Engineers at design@digikey.com.


Weather Center Live Data


The table below is the collection of the data from the weather center structure and its sensor nodes. Each sensor node that has been developed is indicated by the Node name (Node_x) which may or may not have multiple sensors attached to it. In this example each node will transmit the type(s) of sensor(s) it is along with the corresponding data of that sensor. The data that is collected by each sensor is periodically transmitted to a database via a XML file. This XML file is then used to create the following table. Heat Index and Dew Point are calculated using measurements from the table and are not recorded by sensors. Although the Weather Center and the sensors mounted to it strive to bring you the most accurate information possible it does not follow the guidelines set forth by NOAA. This can result in differences between sensor readings on this website and readings on other websites and can also result in differences between similar sensor readings on this website. As these sensors are on the roof, temperatures during the summer months may read as higher than expected.

Node SI Unit SI Value US Unit US Value Time Stamp
DKWS.Node_0 Battery Current A 0.41 A 0.41 06/17/2011 4:13:16 PM
DKWS.Node_0 Battery Voltage V 10.73 V 10.73 06/17/2011 4:24:32 PM
DKWS.Node_0 Solar Current A 0.11 A 0.11 06/17/2011 4:20:46 PM
DKWS.Node_0 Solar Voltage V 5.28 V 5.28 06/17/2011 4:17:02 PM
DKWS.Node_1 Pressure hPa 967 inHg 28.53 03/16/2012 7:50:49 AM
DKWS.Node_1 Temperature C 65 F 149 03/16/2012 7:50:49 AM
DKWS.Node_1 Humidity % 50 % 50 03/16/2012 7:50:49 AM
DKWS.Node_2 Temperature C 45 F 113 03/16/2012 7:43:28 AM
DKWS.Node_2 Light Lux 247 Lux 247 03/16/2012 7:43:28 AM
DKWS.Node_3 Wind Speed Kph 12 Mph 7.456 03/16/2012 7:50:53 AM
DKWS.Node_3 Wind Gust Kph 15 Mph 9.321 03/16/2012 7:50:53 AM
Heat Index C 73.33 F 164 03/16/2012 7:43:28 AM
Dew Point C 32.19 F 89.94 03/16/2012 7:43:28 AM

Current Weather Conditions Image
This image was taken by a USB webcam configured to work with the beagleboard. This node is also located on the back of the weather center structure periodically uploading images to view.

Connectivity Home | Questions?